Booting Android 10 using TFTP/NFS on i.MX8MQ-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting Android 10 using TFTP/NFS on i.MX8MQ-EVK

1,525 次查看
pradeep2481
Contributor II
Hi,
 
I need some help related to i.MX8MQ-EVK.
 
I am trying to boot Android 10 through TFTP /NFS on an i.MX8MQ-EVK platform.
Based on my knowledge, to boot android using TFTP/NFS we need the following changes.
1. Kernel configuration changes to support NFS mount
2. Changes in the init binary
3. Changes in the  init scripts.
 
Changes in the kernel is straight forward and I have identified it and it is working fine.
But for the changes in the init and init.rc I am not sure what exactly needed.
It would be great If I can get some input regarding the changes needed for the init and int scripts.
 
Also What about the SELinux policies? Do we have to change the SELinux policies since we boot from NFS?
 
Thanks in advance,
 
Best regards,
Pradeep
2 回复数

1,507 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately @pradeep2481 , this is not an option from NXP to provide help in the use of  Android with NFS Mounting to avoid secure breach.

 

0 项奖励
回复

1,497 次查看
pradeep2481
Contributor II

@jamesbone, It is for automated test purpose, not for any development.

0 项奖励
回复