Boot is delayed 30 seconds on cold boot imx8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot is delayed 30 seconds on cold boot imx8

2,214 Views
Amelius
Contributor I

Hey,

I'm experiencing a strange behavior during a cold start up (the device is disconnected from power longer than 2 Minutes and than powered up). The boot up is delayed right after "ddrc freq set to low bus mode" by 30s twice (see log) and the total boot time is around 80s.

If the device is rebooted or just unplugged and plugged for less than 20 seconds, the boot time is around 15s

Processor: i.MX 8M

Greetings

0 Kudos
Reply
4 Replies

2,204 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

@Amelius 

Does this issue exist on customer board?

0 Kudos
Reply

2,196 Views
Amelius
Contributor I

Yes, it's a customer board

0 Kudos
Reply

2,187 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

2,119 Views
Amelius
Contributor I

After further investigation I came to the conclusion that the behavior occurs after adding the RT kernel patch patch-5.4.3-rt1 and the kernel config options CONFIG_EMBEDDED=y and CONFIG_PREEMPT_RT=y

adding 
CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE=y
CONFIG_DEVFREQ_GOV_PERFORMANCE=y
didn't bring an improvement

it doesn't look like it has to do with the ddr hardware design since the manufacture did extensiv tests with the mentioned tool

Index of /pub/linux/kernel/projects/rt/5.4/older/

0 Kudos
Reply