Boot iMX 8M mini from nor flash via ECSPI2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot iMX 8M mini from nor flash via ECSPI2

Jump to solution
1,898 Views
CraigTsai
Contributor I

Hi expert,

We plan to boot from spi nor flash via ECSPI2 on iMx8 mini and do some research from community.

The following information is collected :

https://community.nxp.com/t5/i-MX-Processors/Boot-from-SPI-NOR-on-iMX-8M-Mini/m-p/1046463

https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8M-mini-LPDDR4-via-flash-conencted-to-ECSPI2/m...

Here has some question need you to provide more information:

1. Should spi nor bootloader can be use the same binary with SD card interface?

    If don't, how to generate a bootloader form spi nor flash via ecspi boot.

2. How to use uuu to burn this bootloader to spi nor? Should example_spinor.uuu can be use directly?

 

Thanks for your reply.

Tags (1)
0 Kudos
Reply
1 Solution
1,890 Views
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
1,624 Views
keerthi-karanth
Contributor II

Hello 

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8. 

 

Any info on the same would be very helpful.

 

Regards

Keerthi

0 Kudos
Reply
1,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

0 Kudos
Reply
1,514 Views
vignesh-baskaran
Contributor III

Hello

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8.

 

Any info on the same would be very helpful.

 

Regards

vignesh

0 Kudos
Reply