Boot iMX 8M mini from nor flash via ECSPI2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot iMX 8M mini from nor flash via ECSPI2

跳至解决方案
1,887 次查看
CraigTsai
Contributor I

Hi expert,

We plan to boot from spi nor flash via ECSPI2 on iMx8 mini and do some research from community.

The following information is collected :

https://community.nxp.com/t5/i-MX-Processors/Boot-from-SPI-NOR-on-iMX-8M-Mini/m-p/1046463

https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8M-mini-LPDDR4-via-flash-conencted-to-ECSPI2/m...

Here has some question need you to provide more information:

1. Should spi nor bootloader can be use the same binary with SD card interface?

    If don't, how to generate a bootloader form spi nor flash via ecspi boot.

2. How to use uuu to burn this bootloader to spi nor? Should example_spinor.uuu can be use directly?

 

Thanks for your reply.

标记 (1)
0 项奖励
回复
1 解答
1,879 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,613 次查看
keerthi-karanth
Contributor II

Hello 

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8. 

 

Any info on the same would be very helpful.

 

Regards

Keerthi

0 项奖励
回复
1,880 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

0 项奖励
回复
1,503 次查看
vignesh-baskaran
Contributor III

Hello

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8.

 

Any info on the same would be very helpful.

 

Regards

vignesh

0 项奖励
回复