Boot iMX 8M mini from nor flash via ECSPI2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot iMX 8M mini from nor flash via ECSPI2

ソリューションへジャンプ
1,874件の閲覧回数
CraigTsai
Contributor I

Hi expert,

We plan to boot from spi nor flash via ECSPI2 on iMx8 mini and do some research from community.

The following information is collected :

https://community.nxp.com/t5/i-MX-Processors/Boot-from-SPI-NOR-on-iMX-8M-Mini/m-p/1046463

https://community.nxp.com/t5/i-MX-Processors/Boot-iMX-8M-mini-LPDDR4-via-flash-conencted-to-ECSPI2/m...

Here has some question need you to provide more information:

1. Should spi nor bootloader can be use the same binary with SD card interface?

    If don't, how to generate a bootloader form spi nor flash via ecspi boot.

2. How to use uuu to burn this bootloader to spi nor? Should example_spinor.uuu can be use directly?

 

Thanks for your reply.

タグ(1)
0 件の賞賛
返信
1 解決策
1,866件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,600件の閲覧回数
keerthi-karanth
Contributor II

Hello 

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8. 

 

Any info on the same would be very helpful.

 

Regards

Keerthi

0 件の賞賛
返信
1,867件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Craig

 

regarding this issue additional details were sent via mail.

 

Best regards
igor

0 件の賞賛
返信
1,490件の閲覧回数
vignesh-baskaran
Contributor III

Hello

 

We are trying to do similar load of bootloader from NOR FLASH via ECSPI2 on iMX8.

 

Any info on the same would be very helpful.

 

Regards

vignesh

0 件の賞賛
返信