Boot configuration for rebooting.(iMX6D)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot configuration for rebooting.(iMX6D)

Jump to solution
1,583 Views
johnciple
Contributor I

Hello,

I am designing with iMX6D.

I will use the IPU1_CSI0 & IPU2_CSI1 at same time.

So. EIM pins will be used for IPU2_CSI1. (8bit Data = EIM_A17~A24(IPU2_CSI1_DATA12~19)), (PIXCLK=EIM_A16),(HSYNC=EIM_DA11),(VSYNC=EIM_DA12)

EIM pins are also used "Boot config".

I can configure EIM pins at power on.

But I can define these pins at software reset.

Do I need to set "boot config" when software reset.

Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,477 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it is necessary to set "boot config" using software reset.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,478 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it is necessary to set "boot config" using software reset.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,477 Views
johnciple
Contributor I

Thanks your answer.

Is the pin that I can know "software reset"?

Thanks.

0 Kudos
Reply
1,477 Views
igorpadykov
NXP Employee
NXP Employee

there is no pin for "software reset"

~igor

0 Kudos
Reply