Boot configuration for rebooting.(iMX6D)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Boot configuration for rebooting.(iMX6D)

跳至解决方案
1,579 次查看
johnciple
Contributor I

Hello,

I am designing with iMX6D.

I will use the IPU1_CSI0 & IPU2_CSI1 at same time.

So. EIM pins will be used for IPU2_CSI1. (8bit Data = EIM_A17~A24(IPU2_CSI1_DATA12~19)), (PIXCLK=EIM_A16),(HSYNC=EIM_DA11),(VSYNC=EIM_DA12)

EIM pins are also used "Boot config".

I can configure EIM pins at power on.

But I can define these pins at software reset.

Do I need to set "boot config" when software reset.

Thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,473 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it is necessary to set "boot config" using software reset.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,474 次查看
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it is necessary to set "boot config" using software reset.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,473 次查看
johnciple
Contributor I

Thanks your answer.

Is the pin that I can know "software reset"?

Thanks.

0 项奖励
回复
1,473 次查看
igorpadykov
NXP Employee
NXP Employee

there is no pin for "software reset"

~igor

0 项奖励
回复