Bluetooth on imx7ulp eval board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bluetooth on imx7ulp eval board

跳至解决方案
3,416 次查看
jaiganesh_sridh
Contributor III

Hello,

I am working with imx7ulp eval board (L4.19.35_1.1.0 SW package) and facing issues in setting up bluetooth module.

As per document "iMX Linux User guide" Section 10 "Connectivity", I am trying to setup bluetooth using the following command and the corresponding log:


root@imx7ulpevk:~# hciattach /dev/ttyLP2 bcm43xx 3000000 flow -b -t 120
bcm43xx_init
Set Controller UART speed to 3000000 bit/s
Failed to update baudrate, command failure
Can't initialize device: Success
root@imx7ulpevk:~#

Is there any step that i am missing ? Please provide your inputs.

Thanks,

Jai Ganesh Sridharan

标签 (2)
0 项奖励
回复
1 解答
3,270 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Unfortunately it is because Linux BSP L4.19.35 was ment for the i.MX7ULP EVKB. i.MX7ULP EVKB has  Murata 1-DX CYW43430 Wi-Fi support instead of QCA9377. So, the BSP has firmware file for CYW43430 instead of QCA9377.

 

You could try with an older BSP L4.14.98, if this is not an option please try contacting murata for software support if they could provide driver for this device.

https://wireless.murata.com/type-1pj.html 

 

Hope this helps,

Best regards,

Aldo.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,268 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Are you using i.MX 7ULP EVK?

Since, unfortunately it is due that our latest Linux BSP is targeted for the i.MX 7ULP EVKB, if possible please try with L4.14.98_2.0.0_ga that you'll find here:
https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.0.0_MX7ULP1&appType=license

 

Also, please note that i.MX 7ULP EVK supports Murata 1PJ (QCA9377-3) Wi-Fi/Bluetooth while EVKB supports Murata 1DX (CYW43430).

 

Hope this helps,

Best regards,

Aldo.

0 项奖励
回复
3,268 次查看
jaiganesh_sridh
Contributor III

Hello Aldo Gutierrez,

Thanks for your response. I found that the chip in my eval board is Murata 1PJ (QCA9377-3). I tried to execute similar command (hciattach /dev/ttyLP2 qca 3000000 flow -b -t 120), but the firmware file is not available in the rootfs:

qca_soc_init: Baud rate changed successfully
File Open (/lib/firmware/qca/tfbtfw11.tlv)
/lib/firmware/qca/tfbtfw11.tlv File Open Fail

I tried building "bitbake firmware-qca9377" in the yocto package but it fails with:

--2020-04-07 12:07:42--  https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-qca-3.0.1.bin
Connecting to 127.0.0.1:3128... connected.
Proxy tunneling failed: Proxy Authentication RequiredUnable to establish SSL connection.

ERROR: firmware-qca9377-3.0.1-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-qca-3.0.1.bin;fsl-eula=true'. Unable to fetch URL from any source.

Can you please let me know from where I could get the firmware file ?

Thanks,

Jai Ganesh Sridharan

PS: By the way, it has been written as "MCIMX7ULP-EVK REV B1" on my iMX7ULP eval board. Does it mean i am using EVK or EVKB ?

0 项奖励
回复
3,271 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Unfortunately it is because Linux BSP L4.19.35 was ment for the i.MX7ULP EVKB. i.MX7ULP EVKB has  Murata 1-DX CYW43430 Wi-Fi support instead of QCA9377. So, the BSP has firmware file for CYW43430 instead of QCA9377.

 

You could try with an older BSP L4.14.98, if this is not an option please try contacting murata for software support if they could provide driver for this device.

https://wireless.murata.com/type-1pj.html 

 

Hope this helps,

Best regards,

Aldo.

0 项奖励
回复
3,270 次查看
jaiganesh_sridh
Contributor III

Hello Aldo Gutierrez,

Thanks. I got the BT working using L4.14.98 BSP package.

0 项奖励
回复