Hi all,
I'd like to confirm the limitation of using i.MX6Q in 1.2GHz.
I have already read following thread but not enough for understand.
https://community.nxp.com/message/624063
In the note of Table 1 said
"If a 24 MHz input clock is used (required for USB), the maximum SoC speed is limited to 996 MHz.”.
On the other hand, In the note of Figure 1 said
"2. If a 24 MHz input clock is used (required for USB), the maximum SoC speed is limited to 792 MHz."
"3. If a 24 MHz input clock is used (required for USB), the maximum SoC speed is limited to 996 MHz.”
https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf
I can't understand that I can use as a 1.2GHz when I input 24 MHz from external Crystal Oscillator.
Q1.
Can I use as a 1.2 GHz when I input 24 MHz from external Crystal Oscillator ?
Q2.
Can I use USB and 1.2GHz in the same time ?
Ko-hey
I have mailed to you and sent the data sheet to you, pls find it