Bluetooth and wifi is not working in android 10 imx8mm board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluetooth and wifi is not working in android 10 imx8mm board

8,431 次查看
shamiullah
Contributor III

Hello @all

I am working on android 10 imx8mm board. Bluetooth and wifi is not working. When i am turning ON the bluetooth, it is showing "Bluetooth is stopping" and i am not  able to turn ON wifi too. With the same hardware, both wifi and bluetooth are working in android 11 but i am facing issues in android 10. Please let me know if any

0 项奖励
回复
6 回复数

7,063 次查看
amul_patel
Contributor I

Hi,

Any update on solution ?

I am facing similar issue and have raised query:

https://community.nxp.com/t5/i-MX-Solutions/imx8qxp-board-Intel-Wi-Fi-6E-AX210-card-Bluetooth-is-not...

 

Thanks,

Amul

0 项奖励
回复

8,426 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Shamiullah

 

for android 10 wifi one can look at below tutorial

Getting Started with NXP-based Wireless Modules on i.MX 8M Quad EVK Running Android 10 OS - User man...

 

Best regards
igor

0 项奖励
回复

8,419 次查看
shamiullah
Contributor III

Hi Igor,

I followed the document  you have shared but still i am facing the same issue.

Can you provide me the following information

  •  In which file it is mentioned the path of Bluetooth and WiFi firmware's? I want to know which firmware does my board use?  Can you please provide the path of the above file?

Thanks & Regards

Shamiullah

0 项奖励
回复

8,414 次查看
igorpadykov
NXP Employee
NXP Employee

>In which file it is mentioned the path of Bluetooth and WiFi firmware's

 

https://github.com/NXP/imx-firmware/tree/lf-5.10.52_2.1.0/nxp

 

Best regards
igor

0 项奖励
回复

8,398 次查看
shamiullah
Contributor III

Hi igor,

Now the wifi is working but bluetooth i am facing the same issue.The firmware is present in brcm/BCM43430A1.hcd path in  target board but i am facing issue while loading the firmware. The log file is attached. Please let me know if any

Thanks & Regards

Shamiullah

标记 (1)
0 项奖励
回复

8,387 次查看
shamiullah
Contributor III

Hi igor,

booting logs:

Bluetooth: hci0: BCM: chip id 94
[ 3.096615] Console: switching to colour frame buffer device 160x50
[ 3.097664] Bluetooth: hci0: BCM: features 0x2e
[ 3.099227] Bluetooth: hci0: BCM43430A1
[ 3.099233] Bluetooth: hci0: BCM43430A1 (001.002.009) build 0000
[ 3.099311] bluetooth hci0: Direct firmware load for brcm/BCM43430A1.hcd failed with error -2
[ 3.099316] bluetooth hci0: Falling back to sysfs fallback for: brcm/BCM43430A1.hcd

Logs in terminal when i turn ON bluetooth

[ 830.841284] init: Untracked pid 2207 exited with status 0
[ 830.860292] binder: release 2162:2201 transaction 105237 in, still active
[ 830.867137] binder: release 2162:2201 transaction 105228 out, still active
[ 830.874359] binder: send failed reply for transaction 105237 to 2151:2152
[ 830.881870] binder: 2151:2152 transaction failed 29189/0, size 4-0 line 3074
[ 830.887991] binder_alloc: 2162: binder_alloc_buf, no vma
[ 830.889259] binder: send failed reply for transaction 105228, target dead
[ 830.894990] binder: 534:554 transaction failed 29189/-3, size 72-0 line 3312
[ 830.964357] binder: undelivered death notification, 0000ea98e9c3e000
[ 830.965112] init: Untracked pid 2217 exited with status 0
[ 830.976502] init: Service 'vendor.bluetooth-1-0' (pid 2151) received signal 11
[ 830.983866] init: Sending signal 9 to service 'vendor.bluetooth-1-0' (pid 2151) process group...
[ 830.993050] libprocessgroup: Successfully killed process cgroup uid 1002 pid 2151 in 0ms
[ 831.001426] init: updatable process 'vendor.bluetooth-1-0' exited 4 times in 4 minutes
[ 831.009575] init: Init cannot set 'ro.init.updatable_crashing_process_name' to 'vendor.bluetooth-1-0': Read-only property was already set
[ 831.022116] init: Init cannot set 'ro.init.updatable_crashing' to '1': Read-only property was already set
[ 831.032264] init: Untracked pid 2220 exited with status 0
[ 832.937623] binder: release 2227:2267 transaction 106999 in, still active
[ 832.944500] binder: release 2227:2267 transaction 106995 out, still active
[ 832.951644] binder: send failed reply for transaction 106999 to 2225:2226
[ 832.958808] binder: 2225:2226 transaction failed 29189/0, size 4-0 line 3074
[ 832.966298] binder: send failed reply for transaction 106995, target dead
[ 833.058439] binder: undelivered death notification, 0000e7e72543e000
[ 836.043588] init: starting service 'vendor.bluetooth-1-0'...
[ 848.589743] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a
[ 848.760764] healthd: battery l=85 v=3 t=35.0 h=2 st=2 c=400 fc=4000000 cc=32 chg=a

 

I am facing the same issue

 

Thanks & Regards

Shamiullah

 

0 项奖励
回复