Bluetooth SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluetooth SDK

1,822 次查看
hjpark71
Contributor III

Hi,

I'm a beginner of using I.Max & bluetooth and need your help..

I plan to make an BT application on I.Max6 + Yocto but I don't know any SDK is the best with them..

my application feature is very simple.. it just send a jpg file to smartphone from I.Max6 board.

Could you recommend me which SDK is most simple and easy to use for this feature..?

I know QT supports BT  but i don't need any graphical interface..

so, I would like to know more light SDK for C or C++ 

thanks a lot..

Best regards,

HJ

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,615 次查看
igorpadykov
NXP Employee
NXP Employee

Hi HJ

please check Chapter 55 Bluetooth® BCM4339 Driver

attached Linux Manual, use bsps and documentation from i.MX6 product page

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process... 

Other bluetooth modules may be needed to port to bsp.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复