Bluetooth Pair error on Android Nougat

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth Pair error on Android Nougat

1,611件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

   I am working on Toradex apalis imx6q with Android Nougat.   When we try remove paired device(bu clicking unpair), still it is in pair list(if it is not refreshed)


Steps::
1.connect the phone via BT.
2.now select "Unpair".

Observation::
it is still in the paired list, if we do refresh then it is removing.

Please provide the fix? 

And also I don't where exactly the proplem come is it from BSP or Application.

Regards,

VinothS

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 返信

1,541件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi vinothkumar,

The could be the app, or some problem with the memory, since you are using toradex bsp please consult with them

Welcome to - Toradex Community 

Regards

0 件の賞賛
返信