Bluetooth Pair error on Android Nougat

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluetooth Pair error on Android Nougat

1,624 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

 

   I am working on Toradex apalis imx6q with Android Nougat.   When we try remove paired device(bu clicking unpair), still it is in pair list(if it is not refreshed)


Steps::
1.connect the phone via BT.
2.now select "Unpair".

Observation::
it is still in the paired list, if we do refresh then it is removing.

Please provide the fix? 

And also I don't where exactly the proplem come is it from BSP or Application.

Regards,

VinothS

Regards,
Vinothkumar Sekar
标签 (2)
0 项奖励
回复
1 回复

1,554 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi vinothkumar,

The could be the app, or some problem with the memory, since you are using toradex bsp please consult with them

Welcome to - Toradex Community 

Regards

0 项奖励
回复