Bluetooth HCI Setup command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth HCI Setup command

ソリューションへジャンプ
4,174件の閲覧回数
tanoue
Contributor III

I would like to make a Bluetooth driver for IW416 chipset on i.MX8M SoC.

 

I read a NXP document  (11.1 Connectivity for Bluetooth wireless technology and Wi-Fi) and a knowledge base then I could use Bluetooth function now.

However, I didn't fully understand how to setup Bluetooth HCI.

 

Please tell me what each command does.

# For PCIe8997/SDIO8997/SDIO8987 and SDIO IW41
hciattach <device> any 115200 flow
hciconfig hci0 up
hcitool -i hci0 cmd 0x3f 0x0009 0xc0 0xc6 0x2d 0x00
killall hciattach
hciattach <device> any -s 3000000 3000000 flow
hciconfig hci0 up 

I wonder why it needs to execute twice "hciattach" and twice "hciconfig hci0 up".

These details are not written in any documentation.

 

Best Regards,

tanoue.

 

0 件の賞賛
返信
1 解決策
4,164件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Recommend you to create thread here https://community.nxp.com/t5/Wireless-Connectivity/bd-p/wireless-connectivity.

Hope can do help for you

Wish you have a nice day

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,165件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Recommend you to create thread here https://community.nxp.com/t5/Wireless-Connectivity/bd-p/wireless-connectivity.

Hope can do help for you

Wish you have a nice day

0 件の賞賛
返信
4,159件の閲覧回数
tanoue
Contributor III
0 件の賞賛
返信