Blhost erase command too long

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Blhost erase command too long

跳至解决方案
1,313 次查看
kensu
Contributor V

Hi 

I use RT1015 and my Flash is W25Q64JVSSIQ.

I use blhost to erase the Flash with USB interface, but the time is very long, it takes about 70 seconds to erase 5MB,

Is it reasonable?

My command is 

blhost.exe -t 300000 -u 0x15A2,0x0073 -- flash-erase-region 0x60200000 0x500000

 

Regards

Ken

标签 (1)
0 项奖励
回复
1 解答
1,298 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,299 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

0 项奖励
回复