Blhost erase command too long

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blhost erase command too long

ソリューションへジャンプ
1,916件の閲覧回数
kensu
Contributor V

Hi 

I use RT1015 and my Flash is W25Q64JVSSIQ.

I use blhost to erase the Flash with USB interface, but the time is very long, it takes about 70 seconds to erase 5MB,

Is it reasonable?

My command is 

blhost.exe -t 300000 -u 0x15A2,0x0073 -- flash-erase-region 0x60200000 0x500000

 

Regards

Ken

ラベル(1)
0 件の賞賛
返信
1 解決策
1,901件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,902件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

0 件の賞賛
返信