Blhost erase command too long

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blhost erase command too long

Jump to solution
1,248 Views
kensu
Contributor V

Hi 

I use RT1015 and my Flash is W25Q64JVSSIQ.

I use blhost to erase the Flash with USB interface, but the time is very long, it takes about 70 seconds to erase 5MB,

Is it reasonable?

My command is 

blhost.exe -t 300000 -u 0x15A2,0x0073 -- flash-erase-region 0x60200000 0x500000

 

Regards

Ken

Labels (1)
0 Kudos
Reply
1 Solution
1,233 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

View solution in original post

0 Kudos
Reply
1 Reply
1,234 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @kensu,

That should be correct, doing some test in this and other boards erasing 5 MB takes around 65 seconds using the UART(115200) or the USB.

Best Regards,

Alexis Andalon

0 Kudos
Reply