BitBurner 1.0.6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BitBurner 1.0.6.0

跳至解决方案
3,479 次查看
chris321
Contributor IV

Hello Freescale Team,

I think ther is a possible Bug in the version 1.0.6.0 of the OTP tool BitBurner.

I'm able to burn the OTP bits of my i.MX283 with version 1.0.5.6, but with 1.0.6.0 it is impossible. If I write a new value to HW_OCOTP_CUST0 with 1.0.6.0 it will not be taken but with 1.0.5.6. it will.

标记 (3)
0 项奖励
回复
1 解答
2,711 次查看
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,711 次查看
alexandresilva
Contributor I

I'm also trying to write some fuses, with this version on IMX280 without success.

Here is the tool's log:

Friday, July 12, 2013 15:00:54

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100001

Read back verify failed. Wrote: 0x00100001 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

0 项奖励
回复
2,712 次查看
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

0 项奖励
回复