BitBurner 1.0.6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BitBurner 1.0.6.0

Jump to solution
2,048 Views
chris321
Contributor IV

Hello Freescale Team,

I think ther is a possible Bug in the version 1.0.6.0 of the OTP tool BitBurner.

I'm able to burn the OTP bits of my i.MX283 with version 1.0.5.6, but with 1.0.6.0 it is impossible. If I write a new value to HW_OCOTP_CUST0 with 1.0.6.0 it will not be taken but with 1.0.5.6. it will.

Tags (3)
0 Kudos
Reply
1 Solution
1,280 Views
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

View solution in original post

0 Kudos
Reply
2 Replies
1,280 Views
alexandresilva
Contributor I

I'm also trying to write some fuses, with this version on IMX280 without success.

Here is the tool's log:

Friday, July 12, 2013 15:00:54

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100001

Read back verify failed. Wrote: 0x00100001 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

0 Kudos
Reply
1,281 Views
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

0 Kudos
Reply