BitBurner 1.0.6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,481件の閲覧回数
chris321
Contributor IV

Hello Freescale Team,

I think ther is a possible Bug in the version 1.0.6.0 of the OTP tool BitBurner.

I'm able to burn the OTP bits of my i.MX283 with version 1.0.5.6, but with 1.0.6.0 it is impossible. If I write a new value to HW_OCOTP_CUST0 with 1.0.6.0 it will not be taken but with 1.0.5.6. it will.

タグ(3)
0 件の賞賛
返信
1 解決策
2,713件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,713件の閲覧回数
alexandresilva
Contributor I

I'm also trying to write some fuses, with this version on IMX280 without success.

Here is the tool's log:

Friday, July 12, 2013 15:00:54

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100001

Read back verify failed. Wrote: 0x00100001 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

StOtpAccessPitc::OtpRegisterWrite() reg_offset=0x19 val=0x00100000

Read back verify failed. Wrote: 0x00100000 Read: 0x00000000

0 件の賞賛
返信
2,714件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try using BitInit from the OTP TOOLs

Note, first, the otp_burner.py script should be used to generate OtpInit.sb file, that

burns OTP bits. Next, the BitInit.exe should be applied to load OtpInit.sb (from

the same directory as the BitInit.exe starts) .

0 件の賞賛
返信