Best way to build Qt on Freescale i.MX2xx platforms with ltib

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Best way to build Qt on Freescale i.MX2xx platforms with ltib

1,682 次查看
jppoulin
Contributor III

Hello gurus,

I am attempting to build a robust build of Qt on the Freescale i.MX embedded platform.

I am now attempting to build for the i.MX25 but after much reading and testing have been very frustrated in properly building Qt on the ltib-based development environment that exists for the MX25.

Q1: Is there a good recipe to build Qt on this embedded platform?

Q2: Which version of Qt should I build for this chip?

Thank you for any hint you can offer... grasping at straws!

   Jean-Pierre

标签 (2)
标记 (2)
3 回复数

1,326 次查看
Yuri
NXP Employee
NXP Employee

The following may be helpful :

https://community.freescale.com/docs/DOC-1481
https://community.freescale.com/message/263854#263854
https://community.freescale.com/message/383642#383642

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,326 次查看
jppoulin
Contributor III

Thank you very much Yuri for taking the time.

In regards to the Yocto build, has anyone been able to build the Mx25 image over Yocto instead of ageing ltib?

Thank you again! :smileyhappy:

0 项奖励
回复

1,326 次查看
Yuri
NXP Employee
NXP Employee

I have no such information :-(

Regards,

Yuri.

0 项奖励
回复