Bare-metal code for iMX6D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bare-metal code for iMX6D

3,770 次查看
kaushalbisht200
Contributor I

We are designing one custom board based on the i.MX6D.

1. We want to use bare-metal environment to check all peripherals, We don't want

   to use the Linux or OS.From where we can get the bare-metal code for iMX6D?

2. Is JTAG is compulsory for the first time boot of the custom board. If yes,

   from where we can by the JTAG otherwise what are the other ways to boot the

   board first time.

标签 (3)
标记 (1)
0 项奖励
回复
5 回复数

3,346 次查看
kaushalbisht200
Contributor I

Thanks for valuable reply. I got the platform SDK.

Yuri from the 2nd point , I mean... When we will get our board. We need to flash the binaries for the first time. So Is it possible to flash the binaries first time on RAW board using USB utilities?

As I know booting is possible in many (SD card, Ethernet, Flash, emmc) ways but during the first time boot, when we will get the new board at that time, How to flash the binaries  on very new board?

0 项奖励
回复

3,346 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  There is special, so called, Manufacturing (MFG) Tools to flash devices using

i.MX6 serial (USB) boot mode.

i.MX 6 Series Software and Development Tool|NXP

Regards,

Yuri.

0 项奖励
回复

3,346 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   generally, the Platform SDK for i.MX6 contains set of stand-alone codes,

but it is not supported more.  Nevertheless, You may provide me Your e-mail

or create request to get the SDK.

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,346 次查看
kaushalbisht200
Contributor I

Thanks Yuri for the reply.

Name :  Kaushal Singh

Mail ID : [email protected]

Yuri, what about my second query...

" Is JTAG is compulsory for the first time boot of the custom board. If yes, from where we can by the JTAG otherwise what are the other ways to boot the board first time."

0 项奖励
回复

3,346 次查看
Yuri
NXP Employee
NXP Employee

Hi,

1.

I have sent link of the SDK.

2.

You may use internal USB bootloader of the i.MX6. The SDK builds
bootable images.

How to build bootable SD image (for i.MX6 SL as example)

Regards,

Yuri.

0 项奖励
回复