BSP sourceCode download link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP sourceCode download link

2,268 Views
Harris
Contributor III

How to find a Linux 3.14 or Linux 4.1 BSP sourceCode download link.

In the following link, there is not a BSP sourceCode。

Embedded Linux for i.MX Applications Processo|NXP

Thanks.

Labels (1)
0 Kudos
Reply
3 Replies

1,955 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

1,955 Views
Harris
Contributor III

Hi, igor,

Thanks.

0 Kudos
Reply

1,955 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

With BSP you  use Yocto Project with repo utility to fetch all the sources (layers) and then, in the process of building an image, you fetch the source packages, build them, etc.

But NXP source code is in http://git.freescale.com/git/

Follow the instructions in Freescale_Yocto_Project_User's_Guide.pdf document to build an image.

Luis

0 Kudos
Reply