BSP sourceCode download link

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BSP sourceCode download link

2,322 次查看
Harris
Contributor III

How to find a Linux 3.14 or Linux 4.1 BSP sourceCode download link.

In the following link, there is not a BSP sourceCode。

Embedded Linux for i.MX Applications Processo|NXP

Thanks.

标签 (1)
0 项奖励
回复
3 回复数

2,009 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

2,009 次查看
Harris
Contributor III

Hi, igor,

Thanks.

0 项奖励
回复

2,009 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

With BSP you  use Yocto Project with repo utility to fetch all the sources (layers) and then, in the process of building an image, you fetch the source packages, build them, etc.

But NXP source code is in http://git.freescale.com/git/

Follow the instructions in Freescale_Yocto_Project_User's_Guide.pdf document to build an image.

Luis

0 项奖励
回复