BSP-bugs in pin routing for LCD parallel interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BSP-bugs in pin routing for LCD parallel interface

1,287 次查看
tomasznowak
Contributor II

Hello,

I'm integrating imx6dl with an LCD (over parallel interface). The problem I encountered were some strange graphical artifacts on the display (blue points etc...).

Further investigation led to concusion that the pad control configuration for some pins of the interface is inproper (should be MX6DL_DISP_PAD_CTL)

Please correct it in the next BSP release.

Affected file: arch/arm/plat-mxc/include/mach/iomux-mx6dl.h

Affected macros: MX6DL_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2 and MX6DL_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10

Best greetings

Tomasz Nowak

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,079 次查看
EgleTeam
Contributor V

We have performed a frammebuffer test and the colors seem to be correct. Besides we can see activity on both nets using a probe. Just in case we're going to modify the macros.

Thanks Tomasz.

0 项奖励
回复

1,079 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Tomasz,

Thank you, let me talk about this with our experts so the correction can be made if needed.

0 项奖励
回复