BSP-bugs in pin routing for LCD parallel interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP-bugs in pin routing for LCD parallel interface

1,712 Views
tomasznowak
Contributor II

Hello,

I'm integrating imx6dl with an LCD (over parallel interface). The problem I encountered were some strange graphical artifacts on the display (blue points etc...).

Further investigation led to concusion that the pad control configuration for some pins of the interface is inproper (should be MX6DL_DISP_PAD_CTL)

Please correct it in the next BSP release.

Affected file: arch/arm/plat-mxc/include/mach/iomux-mx6dl.h

Affected macros: MX6DL_PAD_DISP0_DAT2__IPU1_DISP0_DAT_2 and MX6DL_PAD_DISP0_DAT10__IPU1_DISP0_DAT_10

Best greetings

Tomasz Nowak

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

1,504 Views
EgleTeam
Contributor V

We have performed a frammebuffer test and the colors seem to be correct. Besides we can see activity on both nets using a probe. Just in case we're going to modify the macros.

Thanks Tomasz.

0 Kudos
Reply

1,504 Views
SergioSolis
NXP Employee
NXP Employee

Hello Tomasz,

Thank you, let me talk about this with our experts so the correction can be made if needed.

0 Kudos
Reply