BP Memory Map in i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BP Memory Map in i.MX6

860件の閲覧回数
sugiyamatoshihi
Contributor V

Hi,

Thres is a description 55.9 BP Memory Map and Control Register Definitions innreference manual.

However, it seems BP memory module don't exist as below description.

If there is no function in BP memory, could you remove this, because customer asked how to access these registers.

Table 55-5. Runnable Channel Selection Control

DO Write to DSPOVR register Write to DSPOVR register

55.4.2.3.5 Runnable Channels Evaluation

The functions associated with DO are not available for this device.

Best Regards,

Sugiyama

ラベル(2)
0 件の賞賛
返信
1 返信

764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I will forward Your recommendations to the team.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信