BP Memory Map in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BP Memory Map in i.MX6

1,224 Views
sugiyamatoshihi
Contributor V

Hi,

Thres is a description 55.9 BP Memory Map and Control Register Definitions innreference manual.

However, it seems BP memory module don't exist as below description.

If there is no function in BP memory, could you remove this, because customer asked how to access these registers.

Table 55-5. Runnable Channel Selection Control

DO Write to DSPOVR register Write to DSPOVR register

55.4.2.3.5 Runnable Channels Evaluation

The functions associated with DO are not available for this device.

Best Regards,

Sugiyama

Labels (2)
0 Kudos
Reply
1 Reply

1,128 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I will forward Your recommendations to the team.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply