BOOT_MODE pin reference voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOOT_MODE pin reference voltage

1,660件の閲覧回数
surendrajadhav
Contributor IV

Hello,

i.MX6UL I am referring to BOOT_MODE0 and BOOT_MODE1 for booting purpose. As per datasheet these lines have refernce voltage to  VDD_SNVS_IN.

However in one of the EVK from TechNexion Ltd., I found that BOOT_MODE0 and BOOT_MODE1 pins are reference to 1.8V.

So let me know is it correct what I have done by pulling up BOOT_MODE0 and BOOT_MODE1 to VDD_SNVS_IN.

Regards,

Surendra

ラベル(1)
2 返答(返信)

1,548件の閲覧回数
art
NXP Employee
NXP Employee

Q. So let me know is it correct what I have done by pulling up BOOT_MODE0 and BOOT_MODE1 to VDD_SNVS_IN.

A. Yes, the BOOT_MODE[1:0] pins should be referenced to VDD_SNVS_IN.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,548件の閲覧回数
surendrajadhav
Contributor IV

Thanks Artur.

0 件の賞賛
返信