How to programBoot_Mode[1:0] register to select internal boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to programBoot_Mode[1:0] register to select internal boot

1,416 Views
adityanagal
Contributor III

Hi ,

 

I am working over IMX6 solo processor , as per reference manual  Boot_mode[1:0] should be written 0b10 to select the internal boot. So how to write to write the Boot_Mode[1:0] bits , so processors boot up with Internal boot . Thanks!

 

Regards,

Aditya Nagal

0 Kudos
Reply
1 Reply

1,316 Views
art
NXP Employee
NXP Employee

The SRC_SBMR2[BMOD] register field is read only and cannot be written in software. It just reflects the latched out-of-reset state of the BOOT_MODE[1:0] pins that are configured externally in hardware to define the required boot mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply