BOOT_MODE pin reference voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BOOT_MODE pin reference voltage

1,674 次查看
surendrajadhav
Contributor IV

Hello,

i.MX6UL I am referring to BOOT_MODE0 and BOOT_MODE1 for booting purpose. As per datasheet these lines have refernce voltage to  VDD_SNVS_IN.

However in one of the EVK from TechNexion Ltd., I found that BOOT_MODE0 and BOOT_MODE1 pins are reference to 1.8V.

So let me know is it correct what I have done by pulling up BOOT_MODE0 and BOOT_MODE1 to VDD_SNVS_IN.

Regards,

Surendra

标签 (1)
2 回复数

1,562 次查看
art
NXP Employee
NXP Employee

Q. So let me know is it correct what I have done by pulling up BOOT_MODE0 and BOOT_MODE1 to VDD_SNVS_IN.

A. Yes, the BOOT_MODE[1:0] pins should be referenced to VDD_SNVS_IN.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,562 次查看
surendrajadhav
Contributor IV

Thanks Artur.

0 项奖励
回复