BLE113 UART5 Check

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE113 UART5 Check

3,071 Views
deepanrajanbara
Contributor IV

Hi,

Ours is a custom board based on imx6 and we are faceing  a problem in which the UART5 is connected to BLE113 Bluetooth module and we are able to program the BT module but what we are able to check

Is that the module is it communicating with the board ?

Is there any way to check the debug print in the BT module ?

Thankyou,

Deepanraj.A

Labels (2)
0 Kudos
Reply
6 Replies

2,911 Views
saurabh206
Senior Contributor III

Ok

In this case just verify the Reset configuration of BLE113.

GPIO or power sequence is followed or not.

Saurabh

0 Kudos
Reply

2,911 Views
deepanrajanbara
Contributor IV

Hi Saurabh

Yes Sir Reset configuration & Power Sequence everything has been followed.

Thankyou,

Deepanraj

0 Kudos
Reply

2,911 Views
saurabh206
Senior Contributor III

Hi Deepanraj

Did you able to fixed this issue?

If yes than can you please mention what was the root cause?

Saurabh

0 Kudos
Reply

2,911 Views
deepanrajanbara
Contributor IV

Hi Saurabh,

I am still facing that issue

Deepanraj

0 Kudos
Reply

2,911 Views
saurabh206
Senior Contributor III

Hi

Deeanraj

First verify the RTS, CTS connection is configured properly or not.

You can used the scope for the signal verification.

These are the basic steps.

Thanks

Saurabh

0 Kudos
Reply

2,911 Views
deepanrajanbara
Contributor IV

Hi Saurabh

All the connections are correct and checked every signal all is fine but i dont know how to check the debug print using our BLE113.

Thankyou,

Deepanraj

0 Kudos
Reply