BLE113 UART5 Check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE113 UART5 Check

3,078件の閲覧回数
deepanrajanbara
Contributor IV

Hi,

Ours is a custom board based on imx6 and we are faceing  a problem in which the UART5 is connected to BLE113 Bluetooth module and we are able to program the BT module but what we are able to check

Is that the module is it communicating with the board ?

Is there any way to check the debug print in the BT module ?

Thankyou,

Deepanraj.A

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

2,918件の閲覧回数
saurabh206
Senior Contributor III

Ok

In this case just verify the Reset configuration of BLE113.

GPIO or power sequence is followed or not.

Saurabh

0 件の賞賛
返信

2,918件の閲覧回数
deepanrajanbara
Contributor IV

Hi Saurabh

Yes Sir Reset configuration & Power Sequence everything has been followed.

Thankyou,

Deepanraj

0 件の賞賛
返信

2,918件の閲覧回数
saurabh206
Senior Contributor III

Hi Deepanraj

Did you able to fixed this issue?

If yes than can you please mention what was the root cause?

Saurabh

0 件の賞賛
返信

2,918件の閲覧回数
deepanrajanbara
Contributor IV

Hi Saurabh,

I am still facing that issue

Deepanraj

0 件の賞賛
返信

2,918件の閲覧回数
saurabh206
Senior Contributor III

Hi

Deeanraj

First verify the RTS, CTS connection is configured properly or not.

You can used the scope for the signal verification.

These are the basic steps.

Thanks

Saurabh

0 件の賞賛
返信

2,918件の閲覧回数
deepanrajanbara
Contributor IV

Hi Saurabh

All the connections are correct and checked every signal all is fine but i dont know how to check the debug print using our BLE113.

Thankyou,

Deepanraj

0 件の賞賛
返信