Hi,
Is there a i.MX6 Linux VPU API available for download? All I could find is one for i.MX51.
Thanks,
Mickey.
解決済! 解決策の投稿を見る。
You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE
You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE
Seems like the document you linked to (and others like it for different cores) do not mention the C header file(s) that my application must #include. What is it? And do you have any example/demo code to build with Yocto that uses the VPU API?
In the latest BSP documentation, there is a PDF file i.MX_VPU_Application_Programming_Interface_Linux_Reference_Manual.pdf. You can take this for reference.
Is there a different link to use for this document? Or can anyone attach the bundle to the discussion? When I try to access the page, I get this:
Error 500--Internal Server Error | 
From RFC 2068 Hypertext Transfer Protocol -- HTTP/1.1:10.5.1 500 Internal Server ErrorThe server encountered an unexpected condition which prevented it from fulfilling the request.  | 
Got it! Thanks.