Availability of i.MX6 Linux VPU API

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Availability of i.MX6 Linux VPU API

跳至解决方案
7,421 次查看
MickeyI
Contributor III

Hi,

Is there a i.MX6 Linux VPU API available for download? All I could find is one for i.MX51.

Thanks,

Mickey.

标签 (1)
标记 (1)
1 解答
3,364 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,365 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You can download the document bundle of the BSP. There is a document "i.MX_6Dual6Quad_VPU_API". IMX6_120901_LINUXDOCS_BUNDLE

0 项奖励
回复
3,364 次查看
brainmeltdown
Contributor I

Seems like the document you linked to (and others like it for different cores) do not mention the C header file(s) that my application must #include.  What is it?  And do you have any example/demo code to build with Yocto that uses the VPU API?

0 项奖励
回复
3,364 次查看
jimmychan
NXP TechSupport
NXP TechSupport

In the latest BSP documentation, there is a PDF file i.MX_VPU_Application_Programming_Interface_Linux_Reference_Manual.pdf. You can take this for reference.

0 项奖励
回复
3,364 次查看
maxj
Contributor I

Is there a different link to use for this document?  Or can anyone attach the bundle to the discussion?  When I try to access the page, I get this:

Error 500--Internal Server Error

From RFC 2068 Hypertext Transfer Protocol -- HTTP/1.1:

10.5.1 500 Internal Server Error

The server encountered an unexpected condition which prevented it from fulfilling the request.

0 项奖励
回复
3,362 次查看
Yuri
NXP Employee
NXP Employee

Please try the enclosed.

0 项奖励
回复
3,362 次查看
maxj
Contributor I

Got it!  Thanks.

0 项奖励
回复