Audio input not working on CPU board after connecting Audio board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Audio input not working on CPU board after connecting Audio board

1,262件の閲覧回数
kumarijyoti9994
Contributor II

We are using imx8qxp board(Android Automotive OS) with base board attached. And we have connected the audio board to base board as well. Audio output is working as expected.

However, audio input on CPU board stops working when we connect the audio board.

Please suggest steps on how to enable audio input on CPU board using headphones/earphones.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,234件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If you are using iMX8QXP MEK + base board, the default sound card is CS42888.

Best regards.

0 件の賞賛
返信

1,223件の閲覧回数
kumarijyoti9994
Contributor II

Is there any way to enable input from cpu board when base board is connected?

 

0 件の賞賛
返信

1,219件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hi,

No, when base board it is connected to i.MX8QXP the input audio is through MIC and line inputs.

Best regards.

0 件の賞賛
返信