Assigning multiple IP address for single NIC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assigning multiple IP address for single NIC

1,263件の閲覧回数
lyfsci
Contributor III

Hi Experts,

How to assign multiple ip address to the single NIC interface in the Android 4.4 and 5.0.1 ?

Does it appears in netcfg command ?

Regards,

Lyf

ラベル(1)
0 件の賞賛
返信
1 返信

1,203件の閲覧回数
b36401
NXP Employee
NXP Employee

Yes. It can be done with netcfg command.

Have a great day,

Victor

----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信