Assigning multiple IP address for single NIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assigning multiple IP address for single NIC

1,183 Views
lyfsci
Contributor III

Hi Experts,

How to assign multiple ip address to the single NIC interface in the Android 4.4 and 5.0.1 ?

Does it appears in netcfg command ?

Regards,

Lyf

Labels (1)
0 Kudos
Reply
1 Reply

1,123 Views
b36401
NXP Employee
NXP Employee

Yes. It can be done with netcfg command.

Have a great day,

Victor

----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply