Assigning multiple IP address for single NIC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Assigning multiple IP address for single NIC

1,186 次查看
lyfsci
Contributor III

Hi Experts,

How to assign multiple ip address to the single NIC interface in the Android 4.4 and 5.0.1 ?

Does it appears in netcfg command ?

Regards,

Lyf

标签 (1)
0 项奖励
回复
1 回复

1,126 次查看
b36401
NXP Employee
NXP Employee

Yes. It can be done with netcfg command.

Have a great day,

Victor

----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复