Are there any constraints to setting the DP_EN?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any constraints to setting the DP_EN?

1,706件の閲覧回数
rmeyer_arrow
Contributor II

The Ref Manual says it is only configured on a LP_POR_B, which I can’t find any info on.

Does this mean that the DP_EN bit in the SNVS_LPCR as to be set  the first time that the register is written to.

Does it have to be set within a certain time frame from the first on.

Can it be set then cleared then set again?

Can it be set after something else has been written to that register?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,540件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rick

please look below at example with DP_EN and security document

explaining SNVS in more detailed way.

Q&A: How is mx6 PMIC_ON_REQ under SW control?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,540件の閲覧回数
rmeyer_arrow
Contributor II

Yes I have seen that one and that is my problem there is not delay between the button press and the PMIC_ON_REQ line assert.

0 件の賞賛
返信

1,540件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rick

I am afraid there is no more info regarding this subject.

Best regards

igor

0 件の賞賛
返信