Are there any constraints to setting the DP_EN?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are there any constraints to setting the DP_EN?

1,699 次查看
rmeyer_arrow
Contributor II

The Ref Manual says it is only configured on a LP_POR_B, which I can’t find any info on.

Does this mean that the DP_EN bit in the SNVS_LPCR as to be set  the first time that the register is written to.

Does it have to be set within a certain time frame from the first on.

Can it be set then cleared then set again?

Can it be set after something else has been written to that register?

标签 (1)
0 项奖励
回复
3 回复数

1,533 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rick

please look below at example with DP_EN and security document

explaining SNVS in more detailed way.

Q&A: How is mx6 PMIC_ON_REQ under SW control?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,533 次查看
rmeyer_arrow
Contributor II

Yes I have seen that one and that is my problem there is not delay between the button press and the PMIC_ON_REQ line assert.

0 项奖励
回复

1,533 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rick

I am afraid there is no more info regarding this subject.

Best regards

igor

0 项奖励
回复