Are there any configuration settings needed to make memtool work on the i.MX51 and i.MX53 processors?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are there any configuration settings needed to make memtool work on the i.MX51 and i.MX53 processors?

跳至解决方案
4,880 次查看
joemehigen
Contributor II

We can see the i/o has been memory mapped ok, but memtool always encounters a BUS ERROR trying to access  the GPIO registers.

We're in the process of upgrading Linux from 2.6.35 to 3.14.33.

tls450# cat /proc/iomem

50008000-5000bfff : mmc0

53f80800-53f809ff : /soc/aips@50000000/usbmisc@53f80800

53f84000-53f87fff : /soc/aips@50000000/gpio@53f84000

53f88000-53f8bfff : /soc/aips@50000000/gpio@53f88000

53f8c000-53f8ffff : /soc/aips@50000000/gpio@53f8c000

53f90000-53f93fff : /soc/aips@50000000/gpio@53f90000

53f98000-53f9bfff : /soc/aips@50000000/wdog@53f98000

53fa8000-53fabfff : /soc/aips@50000000/iomuxc@53fa8000

53fb4000-53fb7fff : /soc/aips@50000000/pwm@53fb4000

53fb8000-53fbbfff : /soc/aips@50000000/pwm@53fb8000

53fc0000-53fc3fff : imx-uart

53fdc000-53fdffff : /soc/aips@50000000/gpio@53fdc000

53fe0000-53fe3fff : /soc/aips@50000000/gpio@53fe0000

53fe4000-53fe7fff : /soc/aips@50000000/gpio@53fe4000

53fec000-53feffff : /soc/aips@50000000/i2c@53fec000

63fb0000-63fb3fff : 63fb0000.sdma

63fc4000-63fc7fff : /soc/aips@60000000/i2c@63fc4000

63fec000-63feffff : /soc/aips@60000000/ethernet@63fec000

70000000-efffffff : System RAM

  70008000-70749f33 : Kernel code

  70780000-70d238e7 : Kernel data

f8000000-f801ffff : /soc/sram@f8000000

1 解答
4,352 次查看
joemehigen
Contributor II

Hi Fabio,

I use memtool to access the GPIO and IOMUX registers, makes it easy to setup pad controls and the like.

I created a simple kernel driver to read and write the registers via IOCTLs, and that's working fine.

I plan to look and see how the driver's ioremap differs from mmaps, but development is back on track with this work around.

Thanks

Joe

在原帖中查看解决方案

0 项奖励
回复
10 回复数
4,352 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Joe,

Maybe you could try devmem2 utility for reading the registers?

Take a look at:

http://www.element14.com/community/thread/32436/l/gpio-ports-on-riot-board?displayFullThread=true

Regards,

Fabio Estevam

0 项奖励
回复
4,352 次查看
joemehigen
Contributor II

Hi Fabio,

Thanks for the suggestion.

I still get the same results trying to access a GPIO register.

joe# ./devmem2 0x53f84000

/dev/mem opened.

Memory mapped at address 0x76f8d000.

Bus error

I'll keep investigating.

Thanks again.

Joe

0 项奖励
回复
4,352 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Joe,

What is the specific register you are trying to access and which SoC (mx51 or mx53)?

Regards,

Fabio Estevam

0 项奖励
回复
4,353 次查看
joemehigen
Contributor II

Hi Fabio,

I use memtool to access the GPIO and IOMUX registers, makes it easy to setup pad controls and the like.

I created a simple kernel driver to read and write the registers via IOCTLs, and that's working fine.

I plan to look and see how the driver's ioremap differs from mmaps, but development is back on track with this work around.

Thanks

Joe

0 项奖励
回复
4,352 次查看
joemehigen
Contributor II

The memtool problem occurs on the 2.6 kernel as well as the 3.14 kernel.  It seems to be related to mapping i/o memory.

running memtool on either kernel to an area described in /proc/iomem results in a bus error.

It's more noticeable in the 3.14 kernel because the gpio and iomux areas are now mapped.

Will continue to investigate further.

4,352 次查看
igorpadykov
NXP Employee
NXP Employee

Hi JOE

I think one can try with i.mx53qsb yocto demo images

Public images - fsl-community-bsp/master/440/framebuffer/imx53qsb

Index of /releases/yocto/yocto-1.6/machines/imx53qsb

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,352 次查看
joemehigen
Contributor II

That was our next idea, thanks for the response.

0 项奖励
回复
4,352 次查看
joemehigen
Contributor II

The images on the two links seem to use the 2.6.35 kernel and boot loader, which we have working.

We're trying to upgrade to the 3.14.33 kernel.

I suspect we're having issues setting up the device tree correctly.

Are there images available with a newer kernel?

0 项奖励
回复
4,352 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复
4,352 次查看
joemehigen
Contributor II

Hi Igor,

A quick update, some portions of the chip are accessed fine via memtool.

For instance, the IPU can be read and written fine.

tls450#  memtool 1e04000c 1

Reading 0x1 count starting at address 0x1E04000C

0x1E04000C:  20F90000

tls450#  memtool 1e04000c=20F90000

Writing 32-bit value 0x20F90000 to address 0x1E04000C

I'll check out the link above.

Thanks

Joe

0 项奖励
回复