Arduino interface on MIMXRT1050-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Arduino interface on MIMXRT1050-EVK

4,224 Views
nebulant
Contributor I

Since the Arduino Interface on the MIMXRT1050-EVK is not populated I would like to know what do I need to integrate mzself the hardware on the board. 

I will for sure need the Arduinio stackable header but the question is if I need anz other hardware component to be solded on the board. As I have seen on the schematics there are some 0 Ohm resistors with the label DNP (Do not place) on some of the pins of the header. Do I need to sold them in case I integrate the Arduino Interface?

2 Replies

3,909 Views
nebulant
Contributor I

Thanks for your answer. I will consider then buying this evaluation board and I'll give here a feedback as soon as I test it. Thanks!

0 Kudos
Reply

3,909 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Jorge,

You just need the Arduino stack header.