Any problems leaving JTAG_MOD float?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any problems leaving JTAG_MOD float?

2,027件の閲覧回数
carymednick
Contributor I

It is desired for the production version of a board to allow for boundary scan JTAG operation by default. If needed for software debugging the JTAG_MOD pin will be tied low. This requires leaving the JTAG_MOD pin floating or tying it high. The hardware manual states for normal operation tie the JTAG_MOD pin low. However, it doesn't define what is normal operation. If the JTAG_MOD pin is left floating, will the chip boot and run correctly?

This is a MCIMX6D6AVT10A. However, I think the question is fairly model agnostic.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,814件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cary

according to Table 2-5. JTAG recommendations i.MX6 User Guide IMX6DQ6SDLHDG

JTAG_MOD should be externally connected to GND for

normal operation in a system.

I believe it affects only TAP configuration, no chip behavior on boot or running codes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,814件の閲覧回数
carymednick
Contributor I

Hi Igor,

Thank you for your response. If it only affects TAP configuration than it should not be an issue.

Regards,

Cary

0 件の賞賛
返信