AndroidKK4.4.3_2.0.0-ga u-boot not working on iMx6slevk
Hi,
We are using imx6slevk board and we are using AndroidKK4.4.3_2.0.0-ga kitkat source.We are using 512MB ram so we changed in following file include/configs/mx6slevk.h in the uboot source
/*#define PHYS_SDRAM_SIZE SZ_1G*/
#define PHYS_SDRAM_SIZE (512 * 1024 * 1024).
But this didn't help me nothing log I am able to get after this change also.Is there anything to be done to boot the board.


Hi Srikanth
additionally to these changes it is necessary to run ddr test
https://community.nxp.com/docs/DOC-105652
and update dcd header in uboot/board/freescale/mx6ul_14x14_evk/imximage.cfg
with new calibration settings found from tester.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thanks for your reply and I gone through the link which you have forwarded.So I am trying to download the DDR stress test tool of v2.70 but I am not able to get the link for that can you please forward that link if possible.
Regards,
srikanth
Hi igorpadykov,
Can I get updated imximage.cfg file for android 4.4.3 of u-boot version 2014.04 with 512MB RAM.
Regards,
srikanth.
Hi igor,
Can you please help me I am not able to get success with DDR stress test also.Now how I need to proceed.I tried with DDR v.270 and DDr v1.0.3 also and in both of them test was not successful.
Regards,
srikanth.


Hi Srikanth
for ddr test problems please create new thread.
Best regards
igor