Android wifi function can not pass netperf test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android wifi function can not pass netperf test

4,395 Views
charleshuang
Senior Contributor II

Target O/S: Android

Target Software Package: android_jb4.2.2_1.0.0

Wifi module: intel 4965AGN

We use netperf to measure the performance of wifi function.

And set 500 times continuously and interval of 10 seconds each,but every time it fails

According to test log, the error always occurred while measuring TCP transmission

Could you help to solve this issue?

Labels (4)
Tags (2)
0 Kudos
Reply
9 Replies

3,918 Views
YixingKong
Senior Contributor IV

Charles

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

3,918 Views
danielhung
Contributor III

Hi Yixing,

Yes. We still have this issue. Please help to investigate.

Thanks,

Daniel

0 Kudos
Reply

3,918 Views
max_tsai
NXP Employee
NXP Employee

hi Daniel,

Can you please provide Android log(adb logcat -v time) and kernel log during netpert TCP testing? The attached netperf log only shows TCP/UDP test result, no help to find the cause. Thanks.

Regards,

Max

0 Kudos
Reply

3,918 Views
charleshuang
Senior Contributor II

Hi MaxTsai,

This is logcat and kmsg when Wifi Netperf failed

Please help to investigate.thanks

Regrads

0 Kudos
Reply

3,918 Views
max_tsai
NXP Employee
NXP Employee

hi Charles,

I get no useful information from the log. I think the problem might be related with the configuration of INTEL WiFi driver, like power saving mode. Would you look for the support from INTEL?

I can dig into INTEL driver but I need the environment. Can I know if this module can use in i.MX6 SabreSD? If so, can you lend me the module and the related source code? Thanks,

Regards,

Max

0 Kudos
Reply

3,918 Views
YixingKong
Senior Contributor IV

Daniel

I will branch your post into an internal group and ask en engineer to work on it.

Thanks,

Yixing

0 Kudos
Reply

3,918 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi charles,

Would you please attach the log ?

Best Regards

Dan

0 Kudos
Reply

3,918 Views
danielhung
Contributor III

Hi Dan,

We have already attached the logs for a while. Did you find something from it?

Thanks,

Daniel

0 Kudos
Reply

3,917 Views
charleshuang
Senior Contributor II

Please find enclosed the attachment

if you want to test ,follow the steps below

step 1. run netserver.exe

step  2. modify Test_NetPerf.cmd

               set dutipaddress=192.168.1.108

               set serveripaddress=192.168.1.102

step 3.run Test_NetPerf.cmd , it will generate netperflog.txt .

0 Kudos
Reply