Android vulnerability related with stagefright

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android vulnerability related with stagefright

1,304件の閲覧回数
FangHui
NXP Employee
NXP Employee

There are several vulnerabilities been found recently as below:

    They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.

All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.


To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.

 

Reference:

https://github.com/WhisperSystems/TextSecure/issues/3817

Original Attachment has been moved to: kitkat-stagefright-patch.7z.zip

0 件の賞賛
返信
1 返信

1,106件の閲覧回数
matthiasschaff
Contributor I

will there also be a patch for older versions? Like JB or ICS?

0 件の賞賛
返信