Android vulnerability related with stagefright

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android vulnerability related with stagefright

1,737 次查看
FangHui
NXP Employee
NXP Employee

There are several vulnerabilities been found recently as below:

    They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.

All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.


To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.

 

Reference:

https://github.com/WhisperSystems/TextSecure/issues/3817

Original Attachment has been moved to: kitkat-stagefright-patch.7z.zip

0 项奖励
回复
1 回复

1,539 次查看
matthiasschaff
Contributor I

will there also be a patch for older versions? Like JB or ICS?

0 项奖励
回复