Android vulnerability related with stagefright

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android vulnerability related with stagefright

1,372 Views
FangHui
NXP Employee
NXP Employee

There are several vulnerabilities been found recently as below:

    They are reported as CVE-2015-1538, CVE-2015-1539, CVE-2015-3824, CVE-2015-3826, CVE-2015-3827, CVE-2015-3828 and CVE-2015-3829.

All above vulnerabilities are related with stagefright’s stackoverflow, which exist all android version since JellyBean 4.2. The stagefright is the default Multimedia framework in Android’s AOSP source code.


To avoid attacking toward stagefright, it is recommended to have patches in this attach, which should be applied to myandroid/frameworks/av.

 

Reference:

https://github.com/WhisperSystems/TextSecure/issues/3817

Original Attachment has been moved to: kitkat-stagefright-patch.7z.zip

0 Kudos
Reply
1 Reply

1,174 Views
matthiasschaff
Contributor I

will there also be a patch for older versions? Like JB or ICS?

0 Kudos
Reply