Android usb string descriptors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android usb string descriptors

2,185件の閲覧回数
chandrashekarbs
Contributor I

Hi ,

            I am using imx6qdl sabresd board. When i connect the board to windows machine it is being detected as IMX6Q-SABRESD device in device manager. How to change that string to custom name?

Please help me . Thanks in advance.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,034件の閲覧回数
chandrashekarbs
Contributor I

Hi igor,

           Thanks for the quick response.

We are trying to change the name of the board which is connected to windows machine, not the VID and PID.

Is it possible?

Regards

Chandra

0 件の賞賛
返信

2,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

2,034件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chandra

windows machine uses VID@PID values provided by i.MX6Q ROM,

they are programmed in fuses USB_VID[31:0], USB_PID[31:0]

described in Table 5-10. Fusemap Descriptions i.MX6DQ RM

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Seems there is no way to change them as they are burned in factory.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信